1/16/2019 10:07 AM | |
Posts: 24 Rating: (0) |
Hello, Did somebody find a solution to have a variable as an input for the two the pointer for Put/Get? I'm using PLC 1500. TIA V15. //B ------------------------------------------------------------------------------------------ |
Last edited by: Beginner23 at: 1/16/2019 10:13:57 AMLast edited by: Jen_Moderator at: 1/16/2019 10:37:32 AMNew subject after splitting |
|
1/16/2019 10:19 AM | |
Posts: 2826 Rating: (686) |
I understand that you are desperate to get answers, but it is not helpful to start postings at different places. It cases problems for those who respond. If you insist to continue to do this, I recommend you supply links to all the posts you are asking this question. Responders can then see where progress is made. No enforcement of my opinion is expected. What is NOT an opinion-> (see also: https://support.industry.siemens.com/tf/ww/en/posts/206043/) |
Last edited by: #dP at: 1/16/2019 11:57:29 AMedit after moderator split topic Last edited by: #dP at: 1/16/2019 11:59:05 AM |
|
This contribution was helpful to1 thankful Users |
1/16/2019 10:41 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
Closed cause question posted twice.
|
Follow us on