7/28/2020 12:31 PM | |
Posts: 3 Rating: (0) |
Buongiorno non riesco ad impostare e visualizzare i valori NEGATIVI della temperatura, sul pannello 4TP400/KTP700, acquisiti con la scheda AM2RT2 di una PT100 . Grazie marinsmarins ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/28/2020 13:25:18New subject after splitting |
|
7/28/2020 2:05 PM | |
Joined: 12/18/2014 Last visit: 8/30/2024 Posts: 33646 Rating: (4182)
|
In attachment a example for temperature displaying und setting in a KTP400 with temperature reading on a LOGO! 0BA8.Standard. In LOGO! program scaling the temperature with one decimal place. For exchange the datas between LOGO! and KTP400 using Parameter VM Mapping. You don't write which TIA version and which LSC version you have. This is for why a make With TIA V13 and LSC V8.0 AttachmentTemperature_LOGO!_KTP400.zip (218 Downloads) |
7/28/2020 2:34 PM | |
Posts: 3 Rating: (0) |
Thank you so much, my software is TIA V15.1 BASIC end LSC V8.2.1 |
Last edited by: marinsmarins at: 07/28/2020 14:45:26 |
|
7/28/2020 2:44 PM | |
Joined: 12/18/2014 Last visit: 8/30/2024 Posts: 33646 Rating: (4182)
|
In attachment TIA projekt upgrade to V15.1. AttachmentKTP400 Temperature from LOGO!_V15.1.zip (217 Downloads) |
Follow us on