7/10/2015 9:44 AM | |
Joined: 10/3/2010 Last visit: 5/8/2024 Posts: 1552 Rating: (188) |
Had this issue in V7.0 SP2 (Windows Server 2003 and Windows XP) and now also in V7.0 SP3 Update 6 (Windows Server 2008 R2 and Windows 7). When you have multiple scripts open in VBS-Editor on the WinCC server, it often happens while switching between scripts or saving a script or closing a script, that the Editor is not responding for several minutes. After a while everything is normal again. I've seen this behaviour on multiple systems, so I think it's not PC-related but something inside WinCC. I found an old post from back in 2011 about the same issue already. Is this still a known issue? Any idea's? |
B r g d s , |
|
7/10/2015 2:33 PM | |
Joined: 10/3/2010 Last visit: 5/8/2024 Posts: 1552 Rating: (188) |
Hi Georg, I already had the userdump ready but compressed it's more than 10 mb (limit of attachment)? For now, I made the support request without attachment. They will probably ask to send the file via ftp. |
Last edited by: SteBo at: 7/10/2015 2:35:57 PMB r g d s , |
|
7/28/2015 7:01 PM | |
Joined: 10/3/2010 Last visit: 5/8/2024 Posts: 1552 Rating: (188) |
This service request is still in progress. Requested dumps and logs from Diagnostics Tool are being examined. Although, I noticed similar behaviour in the past on Server 2003 R2, could this be related to following article (MS KB976700)? https://support.microsoft.com/en-us/kb/976700 Meanwhile, I noticed the same behaviour with WinCC Explorer when switching from Graphic Designer Maybe someone has similar issues on Server 2008 R2 (64bit)? |
B r g d s , |
|
7/29/2015 9:32 AM | |
Joined: 10/3/2010 Last visit: 5/8/2024 Posts: 1552 Rating: (188) |
Hi Georg,
Problem happens everytime, doesn't matter if PC is just rebooted or not |
B r g d s , |
|
Follow us on