11/21/2006 6:21 PM | |
Joined: 10/3/2006 Last visit: 3/5/2022 Posts: 44 Rating:
|
Hi experts =) I am currently working on a PCS7 project involvinh WinCC connectivity Pack. For the project, I have made a "SaveAsExcel" function in VBS which is working to my expectations. I am having a hard time converting it to VBA code so that I can run it when clicking a button in WinCC. Any reading materials regarding adjustments in codes from VBS to VBA is greatly appreciated, or any work around will do. Anyway, I have just attached a copy of the VBS code so that you can check whether it is possible or not. Thanks. =) Attachmentexcel.zip (52 Downloads) |
Follow us on