8/15/2022 10:53 PM | |
Joined: 8/14/2022 Last visit: 8/16/2022 Posts: 1 Rating:
|
Hello there I work on a vehicle lift that I have a few difficulties with. Outline: I1: UP-button I2: Down button I6: Counter I7: End stop At the point when I6 + 7 is high, the lift is at the base. At the point when I6 is low and I7 is high, the lift is at its pinnacle. I6 counts for each 15mm. Q1: Hydraulic siphon (lifting) Q2: Lower valves Q4: Warning sound (Below a specific level) I have made a counter capability what begins the admonition sound when it is at a specific level, 150mm. What I really want assistance with: At the point when I bring down the lift, it should stop at a specific level, yet proceed when you push down once more (I2). ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/16/2022 08:27:22New subject after splitting Last edited by: Jen_Moderator at: 08/16/2022 08:28:14Spelling mistake corrected. |
|
8/16/2022 2:14 AM | |
Joined: 12/18/2014 Last visit: 8/7/2024 Posts: 33504 Rating:
|
If you have a program then upload this program as a ZIP file. |
8/16/2022 6:55 PM | |
Joined: 6/11/2019 Last visit: 8/5/2024 Posts: 2207 Rating:
|
Do you mean something like this ? Ella_68 AttachmentSchaltplan5.zip (417 Downloads) |
Follow us on