Industry Online Support
Technical Forum
4/14/2010 10:17 AM | |
Joined: 3/14/2008 Last visit: 9/5/2024 Posts: 2094 Rating:
|
Can somebody verify the correct install of Windows before installing PCS7 7.1? The readme files and "PC configuration and authorization" manuals are so unclear.... Install ES and OS 1. Install XP Proffesional (MUI language) with SP3 (not in domain yet) 2. Install Messaging Queves and IIS 3. Do not update Windows SP3 with new patches 4. Turn off automatic updates 5. Install Intel drivers (v12) because I use Intel network card 6. Set computer name unique name 7. Install Office 2003 with SP3 or Office 2007 with SP2 (optional) but before installing pcs7 8.Make settings to put PC in company domain 9. Install PCS7 7.1 (updates for windows components are automaticallyinstalled) 10. Drink a beer after clean install |
If I could help you, you can use the RATE button. Thank you. |
|
4/19/2010 9:46 AM | |
Posts: 183 Rating:
|
Hello; Last time i inserted my OS in a windows domain was after PCS7 installation, so i think it doesn't matter. |
Follow us on