3/26/2013 6:57 AM | |
Joined: 4/19/2008 Last visit: 9/3/2024 Posts: 1525 Rating: (159) |
Yes, you can Connect 2 Wire Tx to 4 Wire Above mention Input Module Have alook on the Following Manual for the Connection In that Chapter 6.3 Figure no. 6-2 Point No 5 is the Configuration how you can connect it |
Ammy |
|
3/26/2013 7:44 AM | |
Joined: 3/10/2012 Last visit: 4/7/2022 Posts: 62 Rating: (0) |
Yes, you can Connect 2 Wire Tx to 4 Wire Above mention Input Module Have alook on the Following Manual for the Connection In that Chapter 6.3 Figure no. 6-2 Point No 5 is the Configuration how you can connect it hello expert, the manual which you send is not match with the one which i send, once again i wish to conform it. |
3/26/2013 10:19 AM | |
Joined: 3/10/2012 Last visit: 4/7/2022 Posts: 62 Rating: (0) |
dear sir, thank you so much |
10/8/2015 9:42 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4766 Rating: (122) |
New question published by Marko80 is split to a separate thread with the subject How to connect to 6ES7134-4GB11-0AB0?. Best regards |
Follow us on