9/29/2016 9:23 AM | |
Joined: 10/24/2011 Last visit: 6/13/2023 Posts: 71 Rating:
|
Hello guys, I have one little problem with transfer data in DBxx I structured DB with array 0..50 with 110bytes(words) and every conditioned cycle transfer data from DBxx.Position[n] to DBxx.Position[n+1] .... this right run without any problem Now I increase array to 0..80 (total 8910 bytes) and transfer data not correct running Now my question: Is some condition for maximum transfered bytes inside DB´s per one cycle of CPU ??? I tried decrease array to 0..75 (total 8360 bytes) not correct running If I decrease array to 0..74 (total 8250 bytes) transfer of data running correct ??? WHY ??? Have anybody some idea for this ?? Jenda AttachmentDb30_DB31.zip (36 Downloads) |
Follow us on