12/23/2020 1:22 PM | |
Joined: 7/2/2015 Last visit: 6/21/2024 Posts: 96 Rating: (23) |
Hi Pepsi Cola, The Protool an WinCC flexible aren't released to use in a virtualized machine. You can checkit at the Compatibility tool Best regards Troubleshoot_er |
If this Information really helps, you could use the Rate function |
|
12/25/2020 10:23 AM | |
Joined: 3/24/2018 Last visit: 5/5/2024 Posts: 236 Rating: (1) |
This is wrong. The Protool an WinCC flexible are released to use in a virtualized machine with out any problem. |
12/25/2020 12:08 PM | |
Joined: 3/24/2018 Last visit: 5/5/2024 Posts: 236 Rating: (1) |
Hi, Can you explain this procedure in detail ? Iam not do it before. Thank you in advance. |
12/28/2020 2:06 PM | |
Joined: 9/3/2008 Last visit: 10/11/2024 Posts: 928 Rating: (162) |
Hi, About the VirtualBox Extension Pack, you first need to download it from: If you have different version, then look at: https://www.virtualbox.org/wiki/Download_Old_Builds_6_1 https://www.virtualbox.org/wiki/Download_Old_Builds_6_0 |
Michael |
|
This contribution was helpful to1 thankful Users |
Follow us on