5/7/2019 3:26 PM | |
Posts: 10 Rating: (1) |
[snip] My elements are not dinamized with C script, they are dinamized with Dinamic Dialog, and that continue to read the server value... I attach you an example. I tried to write '@local::' before the name but it doesn't work... Regards, Carmen ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/08/2019 08:54:01New subject after splitting. Division of questions into seperate topics. |
|
5/8/2019 8:04 PM | |
Joined: 9/19/2009 Last visit: 5/11/2024 Posts: 458 Rating: (82) |
Hi Do you enable the option of Computer-local of your internal tags? Regards |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
5/9/2019 10:04 AM | |
Joined: 9/19/2009 Last visit: 5/11/2024 Posts: 458 Rating: (82) |
Hi I don´t understand, because you have this option selected, you must have diferent value from the server and the client and you don´t need @local:: By the way @local:: don´t work with dinamic dialog and the new WinCC, however you still can used with VBScript. With dinamic dialog you can use: @NOTP , @NOSP" , @NOP
Regards |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
5/11/2019 6:40 PM | |
Joined: 9/19/2009 Last visit: 5/11/2024 Posts: 458 Rating: (82) |
Hi Did you restart the Runtime of the client? You can´t have the same value... Regards |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
Follow us on