8/14/2018 9:22 AM | |
Joined: 5/12/2006 Last visit: 11/7/2024 Posts: 22439 Rating: (3029)
|
Hello, which Operation System is on the other PC which can use this W10 shared Folder? Regards Christoph |
8/14/2018 11:12 AM | |
Posts: 10 Rating: (0) |
Hello. W10 in one pc and Windows7 in another one. Both work fine. BR, Juaum |
8/14/2018 2:05 PM | |
Joined: 8/3/2009 Last visit: 11/8/2024 Posts: 14127 Rating: (1769)
|
Hello juaum Check the Basics also: https://support.industry.siemens.com/cs/ww/en/view/92346478 Bye Murof |
If this Information really helps, you could use the Rate function |
|
8/15/2018 11:49 AM | |
Joined: 9/3/2008 Last visit: 11/8/2024 Posts: 928 Rating: (163) |
Hi, I just tested a TP700 against a Win10 and it works here. I only tried to get the Windows Explorer on the Panel to access the shared folder on the Windows 10 and it works. What I did is make a directory on Windows 10 called "panel" and share it. I gave the user "panel" Full Rights. On the panel I opened Control panel and in "Network ID" I enter "panel" and the password for this user. You probably need a password. You cannot have an empty password. There is security in Windows that does not allow empty passwords over network. Then I can open Windows Explorer and enter then path \\V15ES01\panel and it gets access immediately. |
Michael |
|
Follow us on