4/27/2008 6:15 PM | |
Joined: 9/27/2006 Last visit: 9/10/2024 Posts: 12282 Rating: (2683) |
Hello kanan; How are you planning to connect the Wago I/O to the S7-315? If through Profibus-DP, then you need to insert the Wago unit's gsd file in the HWConfig editor; it will then appear in the Profibus slave catalog and you can then select and configure it for your application. Have a look at the followingdocument from Wago: http://www.wago.com/wagoweb/documentation/app_note/a2022/a202201e.htm Hope this helps, Daniel Chartier |
4/28/2008 6:10 AM | |
Posts: 133 Rating: (2) |
thanks guys for support! But I have download GSD file for profibus communication and installed it but still can not see wago i/o in HW configuration?? may be i downloaded something wrong? see attached pictures. Regards Attachment1.zip (415 Downloads) |
4/28/2008 8:49 AM | |
Posts: 2348 Rating: (264) |
kanan, maybeyouareright,butstillithinkthissubjectisforwagoforum. Don'tgetoffended-it'sjustIMHO. |
4/28/2008 9:58 AM | |
Posts: 133 Rating: (2) |
Dear jecek d thanks! I did what you said and now i can see wago in hw. conf.! regards! |
Follow us on