12/1/2018 9:52 AM | |
Posts: 22 Rating: (0) |
Hi everybody , I want to change the range of IP Address in CPU 319F-3PN/DP. In this case we have also D445. now I changed the range in PLC . (from 192.168.1.2 to 172.27.119.2 ). In Simotion D445 we have 3 IP Addresss. I want to change their IP Address like this: 1) 192.168.1.4 to 172.27.119.4 2) 192.168.2.1 to 172.27.119.200 3) 169.254.11.22 to 172.27.119.201 Now, Can I change number 2 and number 3 in Simotion, with this ranges ( 2)192.168.2.1 to 172.27.119.200 3)169.254.11.22 to 172.27.119.201 ) I want to know Is this allowed? and if no, what should I do to changing with (192.168.2.1 & 169.254.11.22 ) ? thanks for your reply. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/3/2018 1:59:27 PMNew subject after splitting |
|
12/4/2018 10:25 AM | |
Joined: 5/12/2006 Last visit: 10/15/2024 Posts: 22414 Rating: (3017)
|
Hello, no is not possible. Regards Christoph |
Follow us on