1/24/2022 12:08 PM | |
Joined: 9/6/2021 Last visit: 12/13/2022 Posts: 2 Rating: (0) |
Well i have the same problem : I want to install the Sinema RC server on cloud (AWS). But I need to install the version 2.0 (because I want to connect a cp 1243-7 LTE device). But from the version 1.3, there is a dualboot then I can't install the server on AWS. Then do you know if it's possible ? If I can install the server on AWS ? Is that not possible even if I buy a licence ? Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/24/2022 14:21:01New subject after splitting |
|
1/24/2022 3:49 PM | |
Joined: 4/25/2017 Last visit: 7/29/2024 Posts: 427 Rating: (66) |
Hi, SINEMA RC Server in the cloud is only possible from V3.0 or higher. Here is a manual how to do it: |
Best Regards, |
|
1/28/2022 9:55 AM | |
Joined: 8/3/2009 Last visit: 8/7/2024 Posts: 13469 Rating: (1704) |
Hello here are also a few information, but I think unfortunately also only since V3.0 https://support.industry.siemens.com/cs/de/en/view/109801210 Bye Murof |
If this Information really helps, you could use the Rate function |
|
4/26/2024 6:16 AM | |
Joined: 4/2/2021 Last visit: 7/27/2024 Posts: 4 Rating: (0) |
Anyone Success install |
Follow us on