8/27/2014 3:23 PM | |
Joined: 6/20/2011 Last visit: 3/8/2023 Posts: 72 Rating:
|
Helloallmächt!, I want to Change values using the build in webserver, i am busy with my one webpage (No luck so far) the idea is that from the office, some one with acces can change 2 timer values with out using HMI or TIA portal
|
8/28/2014 10:04 AM | |
Joined: 4/22/2010 Last visit: 12/15/2022 Posts: 5697 Rating:
|
Hello, To create a Vat on the webserver you need to: 1 create a Vat in step 7 and save. 2 Rightclick on the Vat and select Object Properties. 3 In the Tab General-Part 2 Check Webserver 4 Go to the hardware configuration, Save and Compile. 5 Download to module. But in a WEB-Vat you can't modify variables. And building a Webpage : Visualization with user-defined web pages on SIMATIC CPUs with PROFINET interface Regards, Marcjan |
Last edited by: Marcjan at: 8/28/2014 10:26 AMLast edited by: Marcjan at: 8/28/2014 10:15 AMProblem solved? |
|
8/28/2014 4:43 PM | |
Joined: 6/20/2011 Last visit: 3/8/2023 Posts: 72 Rating:
|
Hello Marcjan, The Webserve with user defined pages is workking on Step 7 Classic. How ever TIA portal is not working @ the moment.i have a Thread running on this issuehere Thank you, for the wacth table explaination
|
Follow us on