8/21/2020 9:54 AM | |
Joined: 4/28/2015 Last visit: 6/28/2024 Posts: 578 Rating: (43) |
You can find the temperature values under /sys/class/thermal/thermal_zone*/temp. Support for the hardware watchdog is not yet in released image, but the next image release should contain it. You can test the upcoming version by building an own image from https://github.com/siemens/meta-iot2050/, using ./kas-docker --isar build kas-iot2050-example.yml:kas/opt/upstream.yml That's still experimental, and not all features are working yet (specifically mraa / node red I/O is broken). |
This contribution was helpful to1 thankful Users |
8/31/2020 11:11 AM | |
Posts: 5 Rating: (0) |
Hi, question on this topic: is the value of 68000 ok? |
8/31/2020 11:44 PM | |
Joined: 10/24/2019 Last visit: 8/19/2024 Posts: 18 Rating: (1) |
yes the temperature is measured in miliCelcius (mC) 68000 =68.0 °C |
Follow us on