4/19/2016 11:46 AM | |
Joined: 6/3/2014 Last visit: 9/26/2024 Posts: 660 Rating: (193) |
Hello Isas748, i have some ideas. I
would use "Historical Data". Create a Data log and add the 4+ Logging
tags (times and mesaurments). You can log / archive historical data
easily. If you need the mesurements in one line you might need to save
them as .csv and write an exel macro, that sorts them accordingly. Or you could write the data (StartTime, StopTome,
Duration, Measure1..x) into a .csv each time you take a measurement.
Here you can define the structure yourself. You'll need some scripting
for this.
Alternatively
you can use recipes. Create a Recipe with the structure and then fill
the elements with the data (times and measurements). (See "Recipes" in
WinCC TIA Professional or "User archives" in WinCC 7.X). Do
you know how to get ths time? It depends if you want to use the HMI time
or the PLC time. Are there several PLCs saving the measurements or is
it one?
|
~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ★ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ |
|
Follow us on