Industry Online Support
Technical Forum
6/9/2011 10:37 AM | |
Posts: 376 Rating: (57) |
Hello shivam, you use the PLC S5-135U with the CPU928B (order number: 6ES5 928 3UB21). You write: Now as a next step we want to do data logging from the PLC through two ports.PG port on the CPU and profibus port on a module(6ES5-308-3UC11)that’s connected to the CPU.We want to use the profibus port eventually because the pg port is used by the HMI so it’s not available for extended periods. My answer: Unfortunately, I can not solve your problem but I would like to give you the reference to the following documentation. SIMATIC S5-135U/155U System Manual Please notice the chapter 5. Link: http://support.automation.siemens.com/WW/view/en/1085837 I hope you have the manual Programming Guide for the CPU928B. Perhaps you find in this manual important information about your configuration. Topic IM308-C. SIMATIC S5, IM308-C INTERFACE MODULE INCLUDING MEMORY MODULE PROFIBUS-DP MASTER INTERFACE FOR ET 200, TO BE USED WITH S5-115U TO S5-155U Link: http://support.automation.siemens.com/WW/view/en/4037311 best regards Gucci |
Follow us on