11/25/2022 9:41 AM | |
Joined: 5/28/2018 Last visit: 9/25/2024 Posts: 29 Rating:
|
Good afternoon. I need your help . it is necessary to implement weather-dependent temperature control in the heating system on the Logo. There are two temperature sensors, one outside, the second in the heating pipe, there is also a boiler that heats the heating system. I need to make it so that there is a linear graph of temperature changes in the heating system, for example, if it is -20 outside, then the heating system is 95, and accordingly if it is +10 outside, then the heating system will be 40 degrees Celsius. Previously, I used separate control devices to implement this function, and now I decided to do it on the logo, but I can't organize the scaling correctly. Please, if someone has already done this or knows how, you can show an example. |
Last edited by: Jen_Moderator at: 11/25/2022 11:45:21Text formatting optimized. |
|
11/25/2022 12:12 PM | |
Joined: 12/18/2014 Last visit: 3/11/2025 Posts: 34851 Rating:
|
Maybe this can help you ... AttachmentHeating curve.zip (658 Downloads) |
Last edited by: ixo65 at: 11/28/2022 17:17:42 |
|
Follow us on