12/1/2008 10:41 AM | |
Joined: 10/22/2008 Last visit: 2/16/2021 Posts: 59 Rating: (8) |
Hello bocatadeatun, please look at the following FAQ: http://support.automation.siemens.com/WW/view/en/8959853 You can do it in the same way as it is described for WebNavigator V1.1. Amno |
1/8/2009 6:20 PM | |
Joined: 11/25/2007 Last visit: 11/9/2024 Posts: 10 Rating: (0) |
Hi, I have the same problem and the link to FAQ is not found. Please can you help me. Thanks in advance. |
1/9/2009 3:33 PM | |
Posts: 37 Rating: (2)
|
http://support.automation.siemens.com/WW/view/en/8959853 Just in case, here is the text from the FAQ QUESTION: Why do I get the message "can not find #include file filename.h" in Publisher and what can I do about it? ANSWER: According to the WEB NAVIGATOR documentation, the #include instruction is not supported. Remedy: Note: |
9/16/2013 8:55 AM | |
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating: (135) |
New question was splitted to Web Navigator error message Best regards O_Moderator |
Follow us on