1/26/2012 2:05 AM | |
Posts: 2661 Rating: (279)
|
To publish data from OS servers select "server prefix" check box... See section 7.2.5 in the following manual: SIMATIC Process Control System PCS 7 OS Web Option (V7.1) |
1/26/2012 11:46 AM | |
Posts: 1530 Rating: (59)
|
Hello WinCC Man, how about using this: How can I create script functions that are to run on the WinCC Server or WinCC client, but not on the Web Navigator Client? Best regards Bizur |
1/26/2012 5:29 PM | |
Posts: 24 Rating: (0) |
Hello Phantom75, Thanks for your help.
But i do not which server prefix to give in the WebPublisher first window Please give me some more details |
1/27/2012 12:54 PM | |
Posts: 1530 Rating: (59)
|
Hello WinCC Man, ... Christmas ..., it's already such a long time ago, that I can hardly remember. Just a few days work, and here we are again - in treadmill. normally it works this way, that file you want to show has to be reachable via lokal network. In C-Skript you also have to add network adress. E.G. \\Release\data.txt. Your problemwill be, that server file you want to open, also has to be reachable via lokal network and needs to be free. In case of web client this will not work, because you will never find server there. Well, I think we have to look for an object directly in WinCC, which can show texts. Till now, I haven't found one. Maybe you'll find one by your own. Let's post solution here if I/you found something, just to help other users. Best regards Bizur |
Follow us on