8/31/2023 11:42 AM | |
Joined: 7/15/2023 Last visit: 1/16/2024 Posts: 26 Rating: (0) |
Hi all, I'm strugling to make setting the week clock via web working. cam 1 and 2 don't work. When I click a day, it doesn't toggle on/off. cam 3 seems to work fine. I have checked all mappings and tagtable, can't find an error. Attached both logic and web files. Another thing I would like to solve is make variables stick after a uploading LOGO. After powercycle LOGO they stay, but after iploading a changed program they go back to the values in the blocks. Also the clock on the top right doesn't show current date/time on the 'programma' page, but it works fine on the homepage. The webserver is slow, especially when changing to another page. Is this normal or can it be optimised ? Thnx for reading :-) Attachmentsample v1.zip (297 Downloads) |
Last edited by: Domoticom at: 08/31/2023 11:44:03Last edited by: Domoticom at: 08/31/2023 11:47:59 |
|
8/31/2023 12:41 PM | |
Joined: 12/18/2014 Last visit: 8/7/2024 Posts: 33500 Rating: (4162)
|
You already asked here with a similar program. weekly timers on webgui
|
8/31/2023 1:36 PM | |
Joined: 7/15/2023 Last visit: 1/16/2024 Posts: 26 Rating: (0) |
Thnx ! you're right, sorry, I put the project aside and forgor the browser issue :-(
|
Follow us on