9/11/2020 5:24 PM | |
Joined: 12/18/2014 Last visit: 11/18/2024 Posts: 34239 Rating: (4263)
|
So like it is in attachment? |
9/11/2020 6:31 PM | |
Joined: 9/11/2020 Last visit: 1/25/2024 Posts: 24 Rating: (0) |
Yes but then with the astronomical clock the light goes on the day on and not in the evening |
9/11/2020 6:38 PM | |
Joined: 9/11/2020 Last visit: 1/25/2024 Posts: 24 Rating: (0) |
I want it so the light is of durning the day, goes on at sunset and goes of at midnight |
9/11/2020 6:40 PM | |
Joined: 12/18/2014 Last visit: 11/18/2024 Posts: 34239 Rating: (4263)
|
Then make it if my screenshot it shows. |
Last edited by: ixo65 at: 09/11/2020 18:42:42 |
|
9/11/2020 6:59 PM | |
Joined: 9/11/2020 Last visit: 1/25/2024 Posts: 24 Rating: (0) |
Yes but then it uses only the weekley timer right and not the astromatical clock |
9/11/2020 7:45 PM | |
Joined: 9/11/2020 Last visit: 1/25/2024 Posts: 24 Rating: (0) |
Nope, i want only the astronomical clock switch on the light at sunset, and the weekly timer switch of at midnight |
9/11/2020 7:57 PM | |
Joined: 12/18/2014 Last visit: 11/18/2024 Posts: 34239 Rating: (4263)
|
Then try this.... |
Follow us on