9/14/2018 11:49 AM | |
Posts: 2 Rating: (0) |
Hello. I want to read digital input values of logo device. This device will work as modbus server. What are modbus addressees (or offsets) for digital inputs I and digital outputs Q in the LOGO ? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 9/14/2018 1:47:30 PMNew subject after splitting |
|
9/14/2018 1:37 PM | |
Joined: 12/18/2014 Last visit: 7/25/2024 Posts: 33414 Rating: (4147)
|
Attached is an excerpt from the online help.
AttachmentLOGO! 8 Soft Comfort Online-help 2017_11 V8.2 page 60.pdf (329 Downloads) |
2/14/2019 3:29 PM | |
Posts: 3 Rating: (0) |
some example in any programing language |
2/14/2019 3:33 PM | |
Joined: 12/18/2014 Last visit: 7/25/2024 Posts: 33414 Rating: (4147)
|
Hello tec.proativa, at first welcome to the forum. Here's an Siemens example: With LOGO! 8, how do you acquire the measurement data of a SENTRON PAC3200 via Modbus TCP/IP? |
Follow us on