9/7/2009 9:36 AM | |
Posts: 3609 Rating:
|
Import of a Technical Question of an User ashvir wrote: Hi I have a CPU 314 2DP that has profibus DP slaves connected to it. I have another CPU 315 2PN/DP that has profibus DP slaves connected to it. I now want to link both PLC's together on PROFIBUS. I know you have to configure the connection in net pro. One way of doing it is by configuring a S7 connection in net pro and then using BSEND (FB12) and BReceive (FB13) blocks but this connection will only work if a use an additional CP PROFIBUS card on both PLC’s that talks with no DP.1. Is it possible to link both CPU’s together using the existing integrated ports on each CPU that talk Profibus DP. 2. What are the blocks FC1(DP send) FC2(DP receive) used for. |
Follow us on