9/18/2018 7:19 AM | |
Joined: 9/30/2016 Last visit: 7/11/2024 Posts: 914 Rating: (6) |
Hi Ste39, Thank you for answering. I should have mentioned that I tried the "go to location" already but as far as I can see the current place is the only place the coil is written to - see the attached screenshots. I am almost sure that the coil is controlling a valve and that this valve IS opened and closed - but I want to see which bits is making that happen and I cannot see that. The "#signals" can only be used inside the block - right? And that is also the reason the "go to location" function does not work on these?
Attachmentmvsv.zip (87 Downloads) |
9/18/2018 8:40 AM | |
Joined: 9/30/2016 Last visit: 7/11/2024 Posts: 914 Rating: (6) |
Hi again Ste39, Thank you for answering. Please also see the attached screenshots. I think you are probably right. But when I search for DB1008.DBX0.0 still nothing pops up?
Attachmentmvs2.zip (81 Downloads) |
9/18/2018 10:08 AM | |
Joined: 9/30/2016 Last visit: 7/11/2024 Posts: 914 Rating: (6) |
Thank you again for answering Ste39 and thank you for answering hdhosseini. Please also see the attached screenshots. So - when I find niether DB1008.DBB0 nor DB1008.DBW0 with the "Go to location" tool the only remaining option is indirect addressing and in that case it is untraceable?
Attachmentmvs3.zip (89 Downloads) |
9/18/2018 11:17 AM | |
Joined: 9/30/2016 Last visit: 7/11/2024 Posts: 914 Rating: (6) |
Hi again hdhosseini, Thank you for answering again. Please also see the screenshots. 1. I tried using the forward search but I don't think I found a place where the tag is activated? 2. How do I sear in the HMI - I tried in the "Tag Management" but am not sure it is the right way? How can I copy the names (to use in the search) from the IDB - when I use control C nothing is copied? 3. I know way too little STL but hope I can wait a little longer with learning it.
Attachmentmvs4.zip (88 Downloads) |
Follow us on