12/5/2018 11:48 AM | |
Joined: 8/25/2014 Last visit: 4/19/2024 Posts: 133 Rating: (1) |
I also have a connection problem between an S7-1200 PLC to a TP700 Comfort panel(1st.gen) In TIA 15 I changed the CPU type from 1214 with version 3.0. to 1214 V4.2 because we changed the PLC. But then I had a problem with the data exchange between the panel and the PLC. The connection to the Panel is established but the panel can't access the Data blocks of the PLC. The memory bits however work. I couldn't make it work so I had to change back to the old PLC. Does anyone know what could be causing this problem that the panel cant read the DB's after updating to V15? Cheers Aleix ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/5/2018 1:35:39 PMNew subject after splitting |
|
12/6/2018 8:59 AM | |
Joined: 8/25/2014 Last visit: 4/19/2024 Posts: 133 Rating: (1) |
Hello. All DB's are accessed symbolically. And all entries in the DB have all ticks Cheers. A |
12/6/2018 9:32 AM | |
Posts: 2826 Rating: (685) |
(3)
|
Follow us on