6/27/2023 1:34 AM | |
Joined: 8/17/2018 Last visit: 7/31/2024 Posts: 4 Rating: (0) |
What Firmware Version do I need on my 416 CPU to accept ET 200MP IO? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/27/2023 09:45:08New subject after splitting |
|
7/2/2023 5:27 AM | |
Joined: 5/28/2008 Last visit: 8/6/2024 Posts: 4515 Rating: (838) |
Hello, Limitation in installed version of SIMATIC is as mentioned here "the IM 155-5 PN HF High Feature interface module can be operated on an S7-400H. Configuration is carried out with STEP 7 V5.5 SP3 and a GSDML file." You have to update your catalog and install all GSD files. For CPU FW, it is always recommended to update FW to the latest FW although previous FW(s) can operate the attached IO modules. |
Last edited by: Ayman Elotaify at: 07/02/2023 05:27:49Ayman Elotaify |
|
10/11/2023 7:45 AM | |
Joined: 9/1/2017 Last visit: 11/22/2023 Posts: 3 Rating: (0) |
Dear Experts, I have existing S7-416 CPU (6ES7 416-3ER05-0AB0) with version 5 firmware communicating with ET200M modules on profibus. Now we have to add ET200MP module (6ES7 155-5AA00-0AC0) but we receive error that "firmware version 6.0 for s7-400. Please find attachment for reference. however for S7-416 CPU (6ES7 416-3ER05-0AB0) firmware 5.3 is latest. kindly suggest needful. Attachment416 error.docx (285 Downloads) |
Follow us on