7/10/2023 5:34 PM | |
Joined: 8/12/2022 Last visit: 8/8/2024 Posts: 2 Rating: (0) |
Hi everyone According with this topic, I have some similar issue. Here's an AS with 500 PO's, but our client wanted too add more programming blocks so it generates 128 new PO's (new total: 628 PO's). Unfortunately, we don't have more AS PO licenses. Thanks in advance
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/11/2023 03:54:40New subject after splitting |
|
7/10/2023 5:41 PM | |
Joined: 3/14/2008 Last visit: 11/11/2024 Posts: 2126 Rating: (951)
|
Hi, with AS PO you mean the license on the SEC card? If you exceed that limit, you cannot download the changes... If you are talking about AS RT PO (Runtime PO installed in ALM on the ES station), you can download the changes, but you get a warning during download. Remember that when you upgrade the SEC, you need to do this upfront at least one day. You have to sent the license to Siemens and you get a sort of release file which is installed on the SEC via ALM of the ES. This procedure can take up one day.
|
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
Follow us on