7/26/2013 8:43 AM | |
Posts: 28 Rating:
|
Hello PISCEAN 2010, All i know is from its name It means that FC 15 has 6 input: its name is IN0...IN6 and also 4 output: its name is OUT7...OUT10. The SCL that you wrote not contain any logic explaining about FC 15, it just declare the variable in FC15. It's because when you create FC15 you just named in/temp/out variable as you like. So when you call it in main program you have to declared the variable with PLC's in/out/memory address. Hope this attachment can help, look in chapter 8 regards Shaumi AttachmentS7_GS.pdf (297 Downloads) |
7/26/2013 10:36 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Sorry, I don’t have original back up. Its uploaded. Please find attached here with complete PLC program. I tried to get the information by pressing F1, but it displays in German. This also I tried to translate but couldn’t understand it thoroughly.
Yes it is Siemens block. Its name (header) is POS_AX. I searched in Siemens manual as well as on DocOnCD, but I could not get the details of FC15 as well as other protected FC details.
I too agree with you, but doesnot understand the function of FC. AttachmentD:\PEGARD\Pegard_0.zip (277 Downloads) |
7/26/2013 10:44 AM | |
Posts: 1064 Rating:
|
take a look at this manual pg 207 http://support.automation.siemens.com/WW/view/en/25076613 |
This contribution was helpful to
1 thankful Users |
7/26/2013 10:45 AM | |
Joined: 4/24/2006 Last visit: 3/21/2025 Posts: 8904 Rating:
|
Hello PISCEAN 2010, Perhaps this link might help: Basic logic functions: PLC Basic program powerline (P3 pl) See page 207 Best regards, Wizard |
Last edited by: Wizard at: 7/26/2013 10:46 AMJust typed too slow. |
|
This contribution was helpful to
1 thankful Users |
Follow us on