6/8/2023 10:43 AM | |
Joined: 7/19/2022 Last visit: 8/23/2024 Posts: 380 Rating: (62) |
Hello U_cf7082a6-618f-4..., This is because in the S7-1500 the program is stored on the Memory Card. Therefore, even if you do a factory reset of the PLC, the program will continue on the Memory Card until you delete it. |
If this Information really helps, you could use the Rate function |
|
Follow us on