Industry Online Support
Technical Forum
7/30/2014 1:00 PM | |
Posts: 3609 Rating: (29) |
Import of a Technical Question of the user Anil Mali
|
8/2/2014 9:08 AM | |
Joined: 1/21/2013 Last visit: 6/6/2024 Posts: 4620 Rating: (705) |
Hi Anil Mali, SP = Service Pack Service pack - Wikipedia, the free encyclopedia |
8/2/2014 9:55 AM | |
Posts: 5225 Rating: (1189) |
Hi there. Simatic Manager V5.x SPx is also called here Step7 V5.x. This is the software for designing programs for PLCs (S7-300 / S7-400). WinCC Flexible is software used for creating programs for HMI panels. These are of older genration panels. WinCC V7.0 is used for designing SCADA systems that runs on computers. WinCC have a second licenincing level for the tag count to which the SCADA is allowed to make connection with. As you know the version numbers and service pack numbers indicate the deveopment progress of the software. Some versions are special like WinCC Flexible 2008 SP2 which allow convertion from (very) old panels to newer systems, where WinCC Flexible 2008 SP3 does not have that facility. Siemens has however develop other software since then which aims to work as a unity of modules. The backbone is called TIA Portal. Two modules for this backbone is again called Step7 and WinCC. Please read a very recent related (?) post [LINK]. PLEASE can you be more specific to the reason for your question. If we understand the motivation of your question it might help us to help you the best. Regards. w |
Last edited by: William B. at: 8/2/2014 10:06 AMadd link |
|
Follow us on