7/15/2019 8:46 PM | |
Joined: 4/28/2015 Last visit: 4/21/2024 Posts: 16 Rating: (6) |
Dear expert, hello, 1 - Please lets me know what is the relation between (sinumerik 840D) and (sinumerik PCU50.3). 2- I have a PCU50.3, it means that i have a cnc controller ? thanks very mutch.
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/16/2019 10:58:37New subject after splitting |
|
7/3/2020 2:47 AM | |
Joined: 10/17/2007 Last visit: 5/1/2024 Posts: 3980 Rating: (340)
|
My answer #1--SINUMERIK 840D including basic components and OPTION components for instance, NCU57X.X is basic--you must have it or there will be nothing to do There is NO name as "SINUMERIK PCU50.3", --correct name should be SINUMERIK 840D HMI component PCU50.3, you konw that is an option , but most of the machine builder(99% I think) will select it . it is a special PC running Windows--it is an operator component #2-- PCU50.3,is NOT a cnc controller. DON'T make things confused. someone talking about old SINUMERIK 840Di, that is already discontinued by Siemens. Also that one using PCU50 NOT PCU50.3, the software installed is different than normal PCU 50, and there is MCI card insert inside PCU50 PC slot
|
If you like my comments please |
|
Follow us on