10/16/2023 4:48 AM | |
Joined: 3/30/2020 Last visit: 8/7/2024 Posts: 4670 Rating: (969)
|
The S7-1200 is able to generate up to 4 pulse train outputs that can be used for control of servo / stepper motors. See the PTO section in the hardware configuration. The motion control technology object is used for the controls. Note that only onboard transistor outputs can be used. For this case, outputs from the signal board can also be used. As the previous volunteer Gustavo Banchetti mentioned, other control methods are made available for motion control. These are communications and analog. Does these notes answer your query? |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
10/16/2023 7:15 AM | |
Joined: 9/13/2023 Last visit: 10/18/2023 Posts: 35 Rating: (0) |
I didn't understand what the main role of the TM module is or when it should be used. |
10/16/2023 2:04 PM | |
Joined: 3/30/2020 Last visit: 8/7/2024 Posts: 4670 Rating: (969)
|
The S7-1200 does not have a TM Pulse module. The ET200 product range however does have such a type Technology Module (https://support.industry.siemens.com/cs/document/109479718/). The S7-1500 PLC range also have Technology Modules. For these PLC ranges you must have a TM to do these special tasks.. unless the S7-1500 Compact type CPU is used. Which part number do you have in mind? |
Last edited by: qwazee at: 10/16/2023 14:05:13Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
Follow us on