2/9/2022 2:17 PM | |
Joined: 3/11/2019 Last visit: 7/26/2024 Posts: 1528 Rating: (271) |
Hi, there is a note in an FAQ available i have found. What options are there in STEP 7 (TIA Portal) for backing up projects and what is the significance of the backup files of the projects?-> "Significance of the backup files" "STEP 7 (TIA Portal) creates copies from parts of older project data, which are managed intra-system by the TIA Portal. The TIA Portal creates the backup folder during configuration only after extensive changes have been made. However, the files contained in it are not suitable for a complete restoration." "These backup files are not backup files of the archive function and cannot be used for manual restoration of STEP 7 (TIA Portal) projects. Send the project toTechnical Supportif you can no longer operate the project because of data loss. To do this, pack the project directory together with the backup directory into a ZIP file and use the Support Request." regards sancruz |
Last edited by: sancruz at: 02/09/2022 14:19:29Feedback appreciated, please rate |
|
This contribution was helpful to3 thankful Users |
Follow us on