3/20/2024 10:47 AM | |
Joined: 2/6/2009 Last visit: 6/10/2024 Posts: 46 Rating: (23) |
I also need help with Simatic Logon licensing for WinCC V8. What licenses do I need for 2 OS Redundant servers and 2 OS Clients in order to use simatic logon on WinCC V8? In industry mall there is no entry for Simatic logon for WinCC V8, but MLFB are the same on WinCC TIA Professional and on PCS7 pages, so I guess that the licenses are the same. Do I need license 6ES7658-7BX61-0YA0 for each PC, both servers and both clients? Or just for the servers? Best regards, VladD ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/21/2024 08:44:19New subject after splitting |
|
Follow us on