11/10/2020 6:07 AM | |
Joined: 12/18/2014 Last visit: 4/28/2024 Posts: 32898 Rating: (4067)
|
Import of a technical question via PM from the User Azalia.Az Hi Ixo65, I have a question regarding to LOGO soft V8 license. If customer purchase one DVD, can it be installed on multiple PC at the same time with full license. If yes, what does "1 INSTALLATION" and "Single license" mean as per product description. Thank you in advance. |
Follow us on