5/6/2019 2:22 PM | |
Posts: 5 Rating:
|
Hello Sir, I am trying to communicate s7 200 smart PLC with v90 PTI drive through Modbus RTU communication. In Speed Control mode it works absolutely fine without any issue but in IPOS its not taking position I have give values to 40100,40101,40102 & 40103. I want to know what parameters setting needed to be done for the position and for IPOS mode 50 pin cable from CPU to drive is necessary or not ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/06/2019 14:33:19New subject after splitting |
|
5/7/2019 11:04 AM | |
Joined: 10/11/2006 Last visit: 7/12/2024 Posts: 5874 Rating:
|
Dear Prutha Did you follow the existing application example for positioning with modbus ? The section 7.7.2 describes the modbus communication in general, whereas section 7.7.2.2 in the third example the communication for modbus and positioning is described. |
With best regards, |
|
Follow us on