11/18/2021 11:03 AM | |
Joined: 3/14/2008 Last visit: 7/25/2024 Posts: 2079 Rating: (931)
|
Hi, When you have created a copy of the block icon, go to the properties of the block icon->System->Type and remove only the "@" from the value. For example you have a OpDi01 with type: @OpDi01/3 if you have a copy just delete the "@" so you end up with: "OpDi01/3". Then the wizard will not delete the block icon from the screen. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on