8/24/2013 1:15 AM | |
Joined: 9/27/2006 Last visit: 1/15/2025 Posts: 12328 Rating: (2699)
|
Hello Sam; From the System and Standard Functions manual, System Software for S7-300/400 System and Standard Functions Volume 1 and Volume 2
27.3 Date and Time as Complex Data Types Actual Parameters for DATE_AND_TIME The DATE_AND_TIME data type falls into the category of complex data types, along with ARRAY, STRING, and STRUCT. The permissible memory areas for complex data types are the data block (D) and local data (L) areas. Because DATE_AND_TIME is a complex data type, when you use DATE_AND_TIME as a formal parameter in a statement, you can provide the actual parameter only in one of the following forms: • A block-specific symbol from the variable declaration table for a specific block • A symbolic name for a data block, such as "DB_sys_info.System_Time", made up of the following parts: - A name defined in the symbol table for the number of the data block (for example, "DB_sys_info" for DB5) - A name defined within the data block for the DATE_AND_TIME element (for example, "System_Time" for a variable of data type DATE_AND_TIME contained in DB5) You cannot pass constants as actual parameters to formal parameters of the complex data types, including DATE_AND_TIME. Also, you cannot pass absolute addresses as actual parameters to DATE_AND_TIME.
|
Follow us on