Industry Online Support
Technical Forum
6/17/2020 7:42 PM | |
Joined: 1/15/2019 Last visit: 1/12/2023 Posts: 8 Rating: (1) |
Hello, I have a similar question/problem. I have a project that I migrated from PCS7 v7 to V9 and I've maintained the old V7 APL and it's working fine in the plant. Now I'm adding a new AS to the project and I want to use the V9 APL, but when I compile and generate the block icons it uses the old library instead of the new one. Is there a way to use the @PCS7TypicalsV8 or do I have to delete the @PCS7TypicalsV7 and recompile? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/18/2020 08:25:36New subject after splitting |
|
Follow us on