2/8/2021 7:35 PM | |
Joined: 1/20/2021 Last visit: 8/30/2022 Posts: 6 Rating: (0) |
HI I am having a similar issue, I am just making sure i am going this right I have my AI input (using RTD1-25N-150-H) going to S7-1200 SM1231 RTD AIx4. I am Pulling the values in the port and using normalize to 0 - 27648 and then scale_x to -50 to 150 (which is the max range of the probes). My issue is when i display the temperature it doesn't look right am I using the Normal X or Scale X Function wrong? Any advice is appreciated. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 02/09/2021 08:18:24New subject after splitting |
|
Follow us on