1/4/2016 8:58 AM | |
Posts: 11 Rating: (1) |
Dear friend I want to make some modification in WinCC flexible for my machine, but I'm wonder when I download my new program to MP277 screen ,are there some parameters will be lost?can you tell me what happen with some setting value if new program is dowloaded ? In my system, the MP277 program assigned in PLC program,I connected to PLC via PC adapter cable.is it possible to online MP277 program in this case( via profibus DP)? Please help me. ------------------------------------------------------------------------------------------ |
Last edited by: CS Moderator at: 1/4/2016 12:10:04 PMNew subject after splitting |
|
1/4/2016 10:50 AM | |
Joined: 4/24/2006 Last visit: 10/15/2024 Posts: 8746 Rating: (1168)
|
Hello pazig, Have a look at the following link: Which connector cables are available for connecting to SIMATIC Panels? There you can find which cables can be used. Best regards, Wizard |
Follow us on