11/4/2020 2:06 PM | |
Joined: 2/23/2017 Last visit: 5/27/2024 Posts: 1 Rating: (0) |
We have a Simotion TIA Portal 15.1 UP5 project with a D455-2 and a PLC 1500SP F where there about 50 axes. This project is a evolution of Simotion Scout classic 5.3 project. Me and my collegues are normally working with the . st source code files because we want to have hystory information with git. Many times one developer works on a module and later another developer uses that module into a different machine project. For this reason we import our .st files into Simotion project very often. This thing works well with Simotion Scout Classic, but not with Simotion Scout TIA Portal. When we import our .st file into Simotion TIA the project.mcp increases his dimetion every time and in two month the project dimention is 10 times bigger then the original. How can we solve this problem? We tried to archive and retrieve the project, but it doesn't help. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/05/2020 08:38:04New subject after splitting |
|
11/6/2020 8:53 AM | |
Joined: 9/23/2005 Last visit: 11/19/2024 Posts: 4796 Rating: (733) |
Have you asked the Siemens support for help as well? Home->mySupport->Support Request |
Last edited by: jacek d at: 11/06/2020 08:54:05Regards, |
|
Follow us on