Industry Online Support
Technical Forum
1/11/2022 5:36 PM | |
Joined: 10/21/2011 Last visit: 8/2/2024 Posts: 26 Rating:
|
I insist! I continue to test Desigo CC 4.0 for evaluation (I am new to this platform, I am in Demo mode and my English is not my native language! Please be patient!). I configured the WebSites and the WebAplication in the SMC and saw the project (both remote client and web client) on another machine on the network and configured a schedule. In the client installed on the server I saw the schedule configured on the remote client. I don't know if it will work but this tells me that both machines are communicating. (see WebAplication.jpg, RemoteClient.jpg, and WebClient.jpg). Now I want to do a similar test with a client installed on another PC. For my first test I left the communication in Unsecured mode. I installed the client. Create a client project and from the SMC I communicate with the server project (I activated it and started it). When I run Desigo CC it tries to connect to the server but closes. A message appears in the Desigo CC Tracer application on the server (see TraceServerwhenClientConnect.png). Something catches my attention, in the client (see ClientManagerDetails.PNG). Please I need help! What can cause this behavior? Could someone clarify for me. Thanks in advance. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/12/2022 09:46:49New subject after splitting |
|
Follow us on