12/20/2021 9:33 AM | |
Posts: 2 Rating: (0) |
hi, When ı select the same plc(cpu), The tıa portal v14 is closing. what is reason? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/20/2021 14:17:31New subject after splitting |
|
12/21/2021 9:31 AM | |
Joined: 10/10/2005 Last visit: 10/18/2024 Posts: 1921 Rating: (136) |
Hello mstfac, is this problem by all PLCs or only by one? Have you opened a project with a CPU or firmware version which is not in the hardware catalog? But TIA Portal should not be closed. Try this procedure with an other project or new generated project. When the same problem occurs then I recommend to new installation of TIA Portal. I recommend also to install the SP1 for TIA Portal V14 and after the update for SP1 first. Delivery release of TIA Portal V14 SP1 Updates for STEP 7 V14 SP1 and WinCC V14 SP1 With best regards |
Follow us on