4/4/2019 7:32 AM | |
Joined: 10/17/2011 Last visit: 7/19/2022 Posts: 148 Rating: (3) |
Hi, I am using s7-1500 cpu 1517F-3PN/DP configured using TIA V15.1 and testing it with simulation software S7-PLC SIM Advanced v2.0 I have KTP400Comfort HMI configured on the same PC. In its connection, communication driver is set to "SIMATIC S7 1500". When I start simulation for HMI, It doesn't work. If I change communication driver to "SIMATIC S7 300/400" under HMI connection then it works. The PG/PC Settings in windows Control Panel are "S7ONLINE(STEP 7)-->PLCSIM.TCPIP.1 Here in PG/PC Settings, I could not found any option for PLCSIM S7-1200 / S7-1500. Please let me know what settings needs to be done for connection communication driver "SIMATIC S7 1500" to work? Thank you, Damayanti ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 4/4/2019 1:18:21 PMNew subject after splitting |
|
4/4/2019 1:40 PM | |
Joined: 10/17/2011 Last visit: 7/19/2022 Posts: 148 Rating: (3) |
Hi, Please find the Advanced PLC SIM Screen shot. What settings I need to do? Thanks, Damayanti |
Follow us on