5/8/2019 4:43 PM | |
Posts: 4 Rating: (0) |
I have a very similar problem... I have two licenses installed, the Step7 Professional and the WinCC Comfort. When I try to add a device in the TIA Portal I get the message that the Portal could not find the Step7 Professional license. (Same error as CJras but with the Step 7 License) As far as I know the TIA Portal should get the license automatically if both is installed. Do you have any ideas why it's not working? Edit: I checked and the WinCC License is activated normally if I add a HMI in TIA Portal. But the Step 7 License just does not do anything, although I can't see any particular difference. The two licenses are on the same drive, have the same license type and validity. Thanks in advance ------------------------------------------------------------------------------------------ |
Last edited by: JustAStudent at: 05/08/2019 17:12:20Last edited by: Jen_Moderator at: 05/09/2019 08:06:12New subject after splitting |
|
5/8/2019 7:32 PM | |
Joined: 5/12/2006 Last visit: 6/7/2024 Posts: 22256 Rating: (2987)
|
Hello, which version? Christoph |
5/9/2019 7:56 PM | |
Posts: 4 Rating: (0) |
Second picture... |
Follow us on