3/20/2020 5:22 PM | |
Joined: 1/12/2017 Last visit: 12/7/2022 Posts: 2 Rating:
|
I am having the same issue, only I am connected through Profinet. I ran a firmware upgrade to V15.1.0.0, which seemed to go fine, then I get this error trying to download the runtime. I can change firmware versions just fine. It is only when I try to download the runtime that I get this error. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/23/2020 09:51:05New subject after splitting |
|
3/26/2020 2:46 PM | |
Joined: 8/3/2009 Last visit: 7/29/2024 Posts: 13392 Rating:
|
Hello you can try to do the Transfer offline with USB Stick: https://support.industry.siemens.com/cs/de/en/view/109740696 check also if you have deactivated the "validate Signatures" in the Transfer Settings in the Panel Settings Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on