1/2/2023 10:20 AM | |
Joined: 1/18/2019 Last visit: 4/17/2024 Posts: 3 Rating:
|
Hi all, I have IOT2050 IP6ES7647-0BAA00-1YA2 FS05, I installed image IOT2050_Example_Image_V1.2.2 on the microSD and it looks like it is booting OK with PWR led green and STAT-led blinking green. I am following the instructions for onboarding, I created the onboarding key by downloading the .cfg file to the USB but when I insert the USB stick into the IOT2050 nothing happens. Something I can't understand is that the instructions mention the MAINT LED and RUN LED, my IOT2050 does not have these LEDs. I have RUN, STAT, USER 1, and USER 2. can someone help me, I'm starting to give up. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/02/2023 12:51:55New subject after splitting |
|
1/9/2023 7:22 AM | |
Joined: 4/28/2015 Last visit: 6/3/2024 Posts: 3345 Rating:
|
Hi, unfortunately I need to tell you that you indeed ordered the wrong device. Your device is a SIMATIC IOT2050, not a MindConnect IoT2050 and therefore you can't use it the way described in the linked documentation. I was told by MindConnect colleagues that you can order the MindConnect IoT2050 only via DI SW pricebook with the ID MP1AXHW00. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
Follow us on